Discussion

Left ArrowBack to discussions page
bchemellibchemelli Posts: 4 Apprentice

I have been successful at writing data to a Modbus device, a Yaskawa controller.  However I can not get data from the Modbus device to the Universal Robot.  I have tried (Using the assignment function) CurrentPos= Modbus_get_signal_status(H_CurrentPos_Int, False).  The signal is setup on the Modbus tab of the installation as a register input. The data type is INT from the Modbus device.

Does anyone have an example of this working?

Thanks,

Ben

Comments

Sign In or Register to comment.
Left ArrowBack to discussions page