Home› Integration
Discussion
Back to discussions page
roehlkk
Posts: 19 Apprentice
How can you get a UR to talk to a Profibus network? |
384 views
|
Answered | |
/ Most recent by roehlkk
in Integration
|
2 comments |

in Integration
Hi all,
I am currently trying to interface with a DMG Mori with a Profibus master robot interface and a DP/DP coupler I am having very little luck getting this set up.
My setup so far is as follows. I have a compact logix PLC talking to the robot via Ethernet/IP the PLC is also talking with an Anybus Xgateway that is setup to be an Ethernet/IP slave on one end and a Profibus slave on the other end. I have the robot to the PLC working, as well as the PLC to the Anybus Xgateway. where I am struggling is getting the Anybus Xgateway to communicate to the machine.
Am I using the wrong hardware? Is there an easier way to do this? Any help would be much appreciated!
I am currently trying to interface with a DMG Mori with a Profibus master robot interface and a DP/DP coupler I am having very little luck getting this set up.
My setup so far is as follows. I have a compact logix PLC talking to the robot via Ethernet/IP the PLC is also talking with an Anybus Xgateway that is setup to be an Ethernet/IP slave on one end and a Profibus slave on the other end. I have the robot to the PLC working, as well as the PLC to the Anybus Xgateway. where I am struggling is getting the Anybus Xgateway to communicate to the machine.
Am I using the wrong hardware? Is there an easier way to do this? Any help would be much appreciated!
Tagged:
Best Answer
-
roehlkk Posts: 19 Apprentice
After looking into the problem in greater detail I found that DMG Mori's documentation was wrong. The DP/DP coupler is for having a Profibus master to Profibus master, the coupler is a slave to both masters. switching my Anybus Xgateway to have a Profibus master on one end and a Ethernet/IP slave on the other end should fix my issues. Anybus part number AB-7800. the PLC is a 5069-L306ER Compactlogix.
https://www.automationworld.com/article/food-and-beverage/connecting-compactlogix-profibus