Good Day,
i wanna locate a small Ring (12mm) with the wrist cam.
I defined a Snapposition with the Calibration board but if i only locatate from there the Position isnt precise enough.
For that i wanna locate a second time closer to the Ring.
The movement to the Part and the Position relativ to the Part is no Problem.
But now i wanna teach the Ring, in that really close Position, without calibrationboard.
How can i do that?
The Ignore_Snapposition fuction does work but the Part is really close and it seems to don`t recordnise the sizedifference because of the much closer distance.
Can somebody help me?
Nicholas_Francoeur