Home› Applications
Discussion
Back to discussions page
lauriefisk
Partner Posts: 2 Recruit
Pin Insertion with Misaligned Hole |
121 views
|
Answered | |
/ Most recent by David_Levasseur
in Applications
|
3 comments |

in Applications
I have an application where I need to test holes for perpendicularity using pin insertion. These holes are meant to be drilled perpendicular to the table surface but are occasionally drilled at an angle. I would like to use the FT sensor with the UR to test these holes. Is there any program or template that can be used in this case? I've browsed the Skills but none seem to do quite what I need.

Tagged:
Best Answer
-
David_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 189 Handy
Hi @lauriefisk,
We currently don't have this function but this is something we are working on.
Unfortunately, I don't have an official release date yet.
David Gariépy
Integration Coach
Comments
-
datarobot Posts: 1 Recruit
I note the FT300 works with UR force mode. Does that mean things like pin insertion are taken care off directly by UR functions now? - https://dof.robotiq.com/discussion/906/perform-lots-of-new-high-precision-force-control-tasks-with-the-new-ft-3000 · TwitterFacebook -
David_Levasseur Beta Tester Beetle Posts: 182 Handy
Indeed @datarobot , you can now use the data from the FT 300 in your force nodes. The Robotiq skills can still help you in many ways however.0 · TwitterFacebook