Home› Programming
Discussion
Back to discussions page
Jose
Posts: 11 Apprentice
How to Start, Stop or Pause program from PLC through MODBUS |
514 views
|
Answered | |
/ Most recent by Jose
in Programming
|
2 comments |

in Programming
Hi guys,
my communication between PLC and robot is done through MODBUS where robot is a slave. Communication through general purpose registers on address 128-255 works fine. For communication I use functions like write_port_register(), read_port_register(), integer_to_binary_list(<value>) to get the register value as a list of booleans (e.g.[True,False,.....]), or binary_list_to_integer(<list>) to go back.
Problem is that I dont know how to connect some boolean from register with action Start, Stop or Pause program. I want to start program from PLC through MODBUS. How are the posibilities to do it ?
With descrete inputs is no problem because on card Instalation - I/O Setup you can link for example digital_in[0] with action Start program but I dont want to do it in this way.
my communication between PLC and robot is done through MODBUS where robot is a slave. Communication through general purpose registers on address 128-255 works fine. For communication I use functions like write_port_register(), read_port_register(), integer_to_binary_list(<value>) to get the register value as a list of booleans (e.g.[True,False,.....]), or binary_list_to_integer(<list>) to go back.
Problem is that I dont know how to connect some boolean from register with action Start, Stop or Pause program. I want to start program from PLC through MODBUS. How are the posibilities to do it ?
With descrete inputs is no problem because on card Instalation - I/O Setup you can link for example digital_in[0] with action Start program but I dont want to do it in this way.
Tagged:
Do you have the ability to send open a socket connection on port 29999 with the robot and send strings? You will need to send the end of line character as well for the command to execute. This also gives you the ability to do other things with the robot such as query state, ensure the robot is ready to have the play command sent for instance or load a different program from the PLC