Home› Integration
Discussion
Back to discussions page
Robotiq_Customer
Posts: 123 Apprentice
What about a gripper and a Denso Robot? |
130 views
|
Answered | |
/ Most recent by Catherine_Bernier
in Integration
|
1 comment |

in Integration
Best Answer
-
Catherine_Bernier Posts: 144 Handy
Hi,
No, it's not exactly the same here is what you need to know:
Hardware Setup
The ROBOTIQ gripper connects to the DENSO RC8 controller via the RS-232 port. You will need to use a RS-485 to RS-232 converter between the ROBOTIQ gripper and the RC8.
COM Port Configuration on the RC8- Operational path: [F6 Settings] – [F5 Communication and Token] – [F3 Data Communication]
- Set communication of device.
- Press [F3 Data Communication] to display the following [Data Communication Settings] window.
-
Select “Serial #1” device option. After selecting the device, press [F5 Edit] key to change its settings.
Edit the serial settings to match the image below.
Including PACscript program to Wincaps III project
Include the Robotiq.pcs program on your project by clicking Add Existing File… under the Project menu. Download the Robotiq.pcs program onto your RC8 controller.
Robotiq Program Structure
Any program that CALLs the Robotiq.pcs subroutine needs have the #include command.
The structure of the Robotic subroutine requires two arguments, a string variable (Command) and a 5 element integer array (Option[]).Command List
To get more details on the commands with examples, check this post here.
Hope this helps.
Robotiq 2-Finger 85&140 Driver - User's Guide
Robotiq 2-Finger 85&140 Driver for RC8
Catherine Bernier, Jr. Eng.