Discussion

Left ArrowBack to discussions page
airmaxairmax Posts: 6 Apprentice
Hello! How can i programm an Helix movement in Z direction?

Best Answer

Comments

  • matthewd92matthewd92 Posts: 462Founding Pro, Tactile Sensor Beta Testers Handy
    This post, http://dof.robotiq.com/discussion/550/how-to-make-a-spiral-motion-on-a-surface-of-5cm-3cm-using-universal-robot , gives an example of a spiral script that allows you to move the arm in a spiral pattern on a plane. We've used this same basic script and given it a z axis component to create a conical helix. You could also modify it slightly to give you a straight helix with a fixed diameter. 
  • airmaxairmax Posts: 6 Apprentice
    Hi Matthew! Thanks for your fast answer. I have seen this post. My problem is more that i want to teach a loop square or circular pattern an when reaching the start/end point to move the tcp in z direction and perform the the loop again. The application will be for rapid protoyping.
  • airmaxairmax Posts: 6 Apprentice
    Hi Matthew! I teached the waypoints with relative postions, also waypoint 1. The movement in z direction works, but when i am moving in process move it will not hold the pattern. It is deviating after every circle in one direction. Is this due to the blend radius?
  • matthewd92matthewd92 Posts: 462Founding Pro, Tactile Sensor Beta Testers Handy
    Try taking waypoint 1 out of the loop. Use it only as a starting point as a fixed waypoint. Make your last relative waypoint be the same location as waypoint 1 when you're teaching. What's happening is waypoint1 is moving over however far it was from the preceding point after each iteration. 
Sign In or Register to comment.
Left ArrowBack to discussions page