Yannik_Methot Handy
Username
Yannik_Methot
Joined
Visits
968
Last Active
Roles
No Roles
Points
107
Reactions
-
Re: Wrist Camera: Visual Offset Tag Dimenisons
Hi @ziga004, Visual Offset Tags are 54x54mm squares with a thickness of about 0.79mm. They also come with adhesive transfer tape to the back of the tag. Hope this helps, (View Post) -
Re: Where to download Driver Package for Robotiq UR5 CB2
Hi @CarlosTheLast You may find archived documents and software on our https://robotiq.com/support/archive website. The driver package to control a 2F gripper over USB-RTU would be DCU-1.0-.10. Hope t… (View Post) -
Re: Grippe 2-F85 Unpowered
Hi @Fernando95, I have opened a support ticket with our team to look at this further as it would likely indicate a gripper failure. YOu will soon receive an answer from us. (View Post) -
Re: Wrist camera error: USB Camera disconnected
Hi @atieng3, If neither LED's are lighting up, it means the issue is specific to the power which can't reach the camera. This could be caused by anything from the robot supplying the 24V to the cable… (View Post) -
Re: Second gripper not recognized
Hi @Vasiliadis, The behavior you are seeing is normal at first since all grippers are at the same communication ID by default so they conflict with each other. Here are some instructions extracted fr… (View Post)