Nicholas_Francoeur Handy
Username
Nicholas_Francoeur
Email
Joined
Visits
312
Last Active
Roles
No Roles
Points
165
Reactions
-
Re: Using variables to skip locations in a pallet.
@iLikeWaffles, absolutely, you can use the pallet counter and increment the value depending on the current value. I have done a quick program showing how it can be done with a 4x3 grid. There is no n… (View Post) -
Re: Configuring Input to Start Program
Remote Control can be enabled from the Settings Menu --> System --> Remote Control. After enabling it, you'll get a menu a the top right of the teach pendant to allow to switch from manual to r… (View Post) -
Re: Writing a script on pendant
@ctiger, let us know how it goes! (View Post) -
Re: Program using dual EOA tooling
Hello @Jstewart, I suggest you have a look at the application builder from UR. When building a machine tending application, you can select a dual gripper option. At the end of the process, you'll be … (View Post) -
Re: Why do we need to hold down the freedrive button for UR?
@newuser, this has been available for as long as I can remember. 1. Wire your switch into the controller 24V and DI0, for example. 2. Go to the installation menu of the Polyscope, and then under IO S… (View Post)