Guillaume_Charron Handy
Username
Guillaume_Charron
Joined
Visits
1,338
Last Active
Roles
Beta Tester Beetle
Points
140
Reactions
-
Re: URCap updated to 1.3.0 kills dashboard server play
Hi all, Indeed, this problem has re-appeared with the Camera URCap version 1.6.6. We have found the root cause of the issue and it will be solved in the next version of the Camera URCap. (View Post) -
Re: Control grippers from Python using MODBUS RTU
Another related post: https://dof.robotiq.com/discussion/92/controlling-the-robotiq-2-finger-gripper-with-modbus-commands-in-python?_ga=2.17431289.1133307955.1542044765-1547192274.1535646624 (View Post) -
FT 300 Sensor: Universal Robots compatibility issue when using PROFINET or Ethernet/IP communication
Hello Pros, Robotiq is aware of a compatibility issue between the FT Sensor URCap (UCS-1.3.0) and UR's Real-Time Data Exchange (RTDE) interface. Activating the Ethernet/IP or Profinet communication p… (View Post) -
Re: Robotiq gripper 2 Fingers - constant Red light
@WalterPintor Thanks for the picture you sent me. We determined that this issue was caused by the installation. It is very important to use low-head screws to mount the 2-Finger Gripper Coupling. Oth… (View Post) -
Re: Error message in RUI
@BenjaminK Below is the correct wiring for our actual Grippers connected to a Robotiq Controller (the 8 wires cable was used with the 2-Finger Gripper Legacy version): White: 485+ A Red: 24V Green: 4… (View Post)