YOSHIHISA Apprentice

Username YOSHIHISA
Joined
Visits 18
Last Active
Roles No Roles
Points 2
Posts
5
Badges
1
Full Name YOSHIHISA KABEYA
Company (optional) KONDOH S/S

Comments

  • Thank you for responding the other day. Thanks to that, the robot hand is running smoothly. I have one more question. When moving the hand, first issue an activation command from the PLC Even if the communication is interrupted now, although it s…
  • Thank you for your reply immediately. It has not worked well yet  I'm thinking of trying a method to directly connect to PLC using RS 485 directly without using a universal controller. Is it possible to connect directly to PLC? Do I need a universa…
  • Thank you for quick response.   https://robotiq.com/support/2f-85-2f-140 I can not find the modbus TCP configuration file on this website I can not change to a Fieldbus , because the PLC does not support only modbus TCP. If you do not have a modbu…
  • Thank you for your reply immediately. I am using modbus tcp type Universal Controller. Since I have confirmed the operation using Robotiq User Interface test software I think that wiring is not wrong. I also confirmed the IP address with PING I …