Home Programming

Discussion

Left ArrowBack to discussions page
mhowemhowe Partner, Wrist Camera URCap 1.3.0 Posts: 41 Handy
Has anyone used a timer to track the amount of time it takes to insert a screw? For example we know it takes 2.5 seconds for the robot to fully insert the screw after it reaches a force in the Z of 50N, Now sometimes the material that is getting the screw is not always the same causing the screw to stop threading early which would mean we hit the force in the Z and the torque of the driver but we still did not reach the depth.

Comments

  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 188 Handy
    Hi @mhowe

    I would use a position instead and screw until the desired position in z is reached. 

    David Gariépy
    Integration Coach
  • mhowemhowe Partner, Wrist Camera URCap 1.3.0 Posts: 41 Handy
    @David_Gariepy How would you go about that when we are doing a find surface to 50N?
  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 188 Handy
    Discussion through mail, will come here later to edit and post solution
    David Gariépy
    Integration Coach
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,250 Handy
    @mhowe we have a screw driving application and we are using both a timer as well as a depth of insertion. We have defined a plane which is where the screws should be installed and the n measure the delta between actual insertion and the plane. If it exceeds a tolerance then we flag the screw as not properly installed and notify the user. Also, if it torques out too soon we notify the user that there was an issue installing the screw. 
Sign In or Register to comment.
Left ArrowBack to discussions page