Home Programming

Discussion

Left ArrowBack to discussions page
MeenCHMeenCH Partner Posts: 3 Apprentice
I want to get string from only the USB bar code scanner ,I try with assignment in operator mode and request_string_from_primary_client("") but it will show the keyboard on the robot screen and need to press the blank to show the cursor before use the bar code scanner.

Actually I try with CB2 robot and it work without touching on robot screen it's also show on screen keyboard but I just scan and the variable got the code number.
but when I use CB3 robot it doesn't work in the same way.
Are there any way to use USB scanner without on screen keyboard.

Comments

Sign In or Register to comment.
Left ArrowBack to discussions page