Discussion

Left ArrowBack to discussions page
SaschaSascha Posts: 2 Recruit

Hi There!

I try to create a thread with UR script language for saving analog_in values (from a sensor) every 0.5 seconds. The values shall all be saved in a vector / table / string ... something similar for processing them afterwards.

My progress so far is as follows:

thread myThread():
i = 1 

z = [] #vector or similar

while True:
z[i] = analog_in(0)
i = i+1

sleep(0.5)  
end
end


Do you know how to solve this Problem?

Thanks a lot for your help!


Best Regards

Sascha

Comments

  • matthewd92matthewd92 Posts: 491Founding Pro, Tactile Sensor Beta Testers Handy
    Lists (arrays, vectors, whatever you call them) are statically sized in UR.  You have to predefine the size of array that you want to use before you can use it.  Then you cannot dynamically change the size of the list while in operation and lists can only be around 250 elements long before there starts to be issues.

    myList = [1,2,3,4,5,6,7.....n] #You have to actually predefine this, it does not care what the values are just so long as there are values
    
    i = 0 #counter for our while loop
    
    
    while i<length(myList):
    
      myList[i] = analog_in(0)
      i=i+1
      sleep(0.5) 
    
    end  

  • SaschaSascha Posts: 2 Recruit
    Hi!

    Thanks a lot for the quick answer!
    You really helped me, my programm is working now.


    Best Regards
    Sascha
  • matthewd92matthewd92 Posts: 491Founding Pro, Tactile Sensor Beta Testers Handy
    You're welcome
Sign In or Register to comment.
Left ArrowBack to discussions page