Discussion

Left ArrowBack to discussions page
cdoeksencdoeksen Posts: 2 Recruit
edited May 16 in Applications
In the future, robotic grinding, polishing, sanding, deburring and finishing applications will be as big as robotic welding.

Robotic grinding, polishing, sanding, deburring and finishing applications growth 17 votes

Yes
100% 17 votes
No
0% 0 votes

Comments

  • cdoeksencdoeksen Posts: 2 Recruit
    Robotic grinding, polishing is a hot space. We just need a little more: (1) standardization + (2) more economic options for active force control and this application will really take off.
  • Etienne_SamsonEtienne_Samson Posts: 356 Handy
    @cdoeksen interesting topic you got there, I vote yes, those application do generate a lot of request and they all represent challenges with big potential. I'm not sure if each one could be as big as welding, but the sum of all them definitively can in my opinion!
    Etienne Samson
    Technical Support Manager - Responsable soutien technique
    +01 418-380-2788 ext. 207
    esamson@robotiq.com
  • Johnson_LiuJohnson_Liu Posts: 10Founding Pro Handy
    Dear Samson, this topic applications that I start to invest in research with Amtru(deburring & polishing) when we got the Cell Phone case polishing inquiry from Jabil Taiwan 2009 (Jabil green point- Jabil is US EMS company - revenue more than 10billion U.S.D), after more than 7 years market growth, now the China market growing quickly, especially the robotic polishing, deburring and grinding, another reason is China lack of the new manpower to join these 3D(difficult, danger and dirty) industries. And government push to improve the automation level to protect environment and healthy. Actually China and Asia still need more qualified SI to join this advanced robotics applications in the future, the market is big and huge that worth for Automation companies to come with us and bring the good results. Johnson Liu from Robotics & 3A Inc. 
Sign In or Register to comment.
Left ArrowBack to discussions page