Discussion

Left ArrowBack to discussions page
SebastienSebastien Posts: 202 Handy
Hi pros,
we are looking at a project where we locate a steel part on a belt conveyor. We tested the parts on a uniform background at the shop. Everything worked fine.

However, the belt ont he conveyor is textures and we are afraid it will not work for the camera. The belt is clean and shows good contrast with the part but the only thing is that it is textured. 

Any tips how to make the camera work on this background? Is is possible to somehow teach the background such that it can be identified and removed in the image analysis?

Tagged:

Comments

  • StudentStudent Posts: 21 Apprentice
    edited April 27
    I am using a camera to detect different parts, not the one from Robotiq but from Cognex. What I did to improve the contrast is mounting a red light, so now I have something like this (not that light but the best image I found on internet):



    But I think that if you have good illumination the texture won't be a problem.
  • Etienne_SamsonEtienne_Samson Posts: 333 Handy
    @Sebastien @Student with the Robotiq wrist camera you should just teach the object on a simple uniform background. When in production you can look at the belt and if the light conditions are good you should be able to set a high detection threshold so that the part is recognized and the background is ignored properly.

    Teaching the object on the textured background is probably not a good idea.
    Etienne Samson
    Technical Support Manager - Responsable soutien technique
    +01 418-380-2788 ext. 207
    esamson@robotiq.com
Sign In or Register to comment.
Left ArrowBack to discussions page