DoF - a Robotiq Community
Warning sign
The Dof Community was shut down in June 2023. This is a read-only archive.
If you have questions about Robotiq products please reach our support team.
Nicolas_Lauzier


Note : This how-to guide was developed for ABB IRC5 controller and Robotiq 3-Finger Gripper generation 5 (sold in 2012-2013).

Robotiq team has gather information to support you in the installation of an electric gripper on an ABB Robot.

Learn how to install an electric gripper on an ABB robot which is using DeviceNet. This information uses the 3-Finger Adaptive Gripper as an example for the installation, see how to set and configure a robotic gripper, detailing everything from hardware installation to communication configuration.

robot gripper electric gripper abb robot

In this ebook you will learn how to:

  • Set up the mechanical interface at the robot's wrist.
  • Configure the DeviceNet network with the end-effector. 
  • Add the unit type to the list of available unit types.
  • Activate the connection to the robot gripper.
  • Map the gripper IO.
  • Program the servo gripper.

So, if you are curious about looking a little more closely into these details, check out this valuable information. Get your ebook here.