Discussion

Left ArrowBack to discussions page
edavioedavio Posts: 2Partner Recruit
Hi pros

Considering to use wrist camera just as coupling plate which connects gripper and a ROS PC. Anyone has experience on it? Can ROS communicate with gripper 85 though wrist camera? Thanks! 

Comments

  • Samuel_BouchardSamuel_Bouchard Posts: 131 Handy
    @Annick_Mottard do you see what @edavio is asking? I was with him at the customer. They have the gripper communicate through the camera (1 cable). Will they be able to use the gripper with ROS in that hardware setting you think?


    CEO & Co-Founder @ Robotiq

    samuel@robotiq.com
  • Annick_MottardAnnick_Mottard Posts: 109 Handy
    @edavio you will be able to use the package. The only thing you need to make sure is that you identify the correct USB device. When you launch the ROS package, it will ask you what USB device to communicate with. Make sure you select the proper one. I you are not sure, you can look at the list of USB devices that are connected. 

    Feel free to post below if you have further questions. 
    Annick Mottard
    Product Expert
    Robotiq
    a.mottard@robotiq.com 
Sign In or Register to comment.
Left ArrowBack to discussions page