Discussion

Left ArrowBack to discussions page
YuuYuu Posts: 3 Apprentice
Hallo, DoF Pros.

I am currently working on a pick and place application using a UR5, 2-Finger Gripper and the FT300 sensor.
Is there are way to robot restart by programs when the robot stops emergency?

Best Answer

Comments

  • YuuYuu Posts: 3 Apprentice
    edited February 27
    @Annick_Mottard, Thank you for your answer.
    After the emergency stop, manually release the emergency stop button.
    After that, is there a method to detect the signal from the PLC and release the abnormal reset?
    Do not use UR 's controller.

  • matthewd92matthewd92 Posts: 488Founding Pro, Tactile Sensor Beta Testers Handy
    There is, you would have to be tied into the real time streaming port and listening for the safety state. It will tell you the exact state the robot is in. You can then restart the robot by streaming events back to the robot. You can also set the robot to automatically start on the rising edge of a hard input (on the robot) so the operators can push a button to reset the robot. 
Sign In or Register to comment.
Left ArrowBack to discussions page