Discussion

Left ArrowBack to discussions page
AfsaarAfsaar Posts: 8Partner Apprentice
Hi all,
when we create two security planes of this kind, the robot will work normally (N) in the middle of the planes and it will go in reduce mode (R) outside. The arrows show where the robot will work normally.

But if we create this kind of planes
the robot will work in reduce mode in each areas, why?
We can't understand why the robot works in reduce mode despite it is in the normal areas.
Afsaar Assenally
Product Specialist

    
Tel. 02 92106011 - Fax. 02 92470439
http://www.alumotion.eu

Best Answers

  • Fionn_MerzFionn_Merz Posts: 1Partner, Beta Tester VIsion 1.1 Program Recruit
    Accepted Answer
    I believe the current implementation of safety planes in the UR makes what you're trying to do impossible. Each plane is considered on it's own, with no consideration of any other planes. This means that in your second example, the plane on the top causes reduced mode to the whole volume below it, and the plane on the bottom causes reduced mode to volume above. So the volume above the top plane is still in reduced mode, because of the bottom plane, and vice versa. In the past we've had to use light curtains instead of safety planes due to this very reason. I hope there's an extension to the safety planes functionality coming, it certainly would be useful for many of our own projects. 

Comments

  • obohigasobohigas Posts: 2Tactile Sensor Beta Testers Recruit
    edited February 9
    Hi!
    How did you specifically set the constraints for the robot to switch to (R) mode?
    Maybe a little more information can help see where the problem is.
    Cheers!
Sign In or Register to comment.
Left ArrowBack to discussions page