Discussion

Left ArrowBack to discussions page
jonlongjonlong Posts: 3 Apprentice
I have a Robotiq 85 2-finger gripper that I'm using with a UR5 running version 3.3.2.266, and would like to control remotely (presumably via URScript).

Perhaps I have missed something basic, but this does not seem to be working, and behaves in ways I would not expect.

When I run "gripper_tutorial.urp" from the pendant, that does work. But when I single-step through any of the rq_* commands (using the >| button on the bottom of the pendant display), I get a compile error, e.g., "Compile error: name 'rq_close' is not defined". Likewise, sending rq_* commands over a socket does not work; there does not seem to be any effect.

I can control the gripper remotely using raw socket commands from URScript, e.g., socket_set_var("POS", 255, "gripper_socket"). But that does not seem to work reliably, and does not seem like the right way to do things given the presence of the rq_* commands.

Any idea what might cause this behavior? Have I missed some initialization step? Shouldn't I be able to send "rq_close()" (e.g.) over a URScript socket?

Best Answer

Comments

  • jonlongjonlong Posts: 3 Apprentice
    Okay, thanks, I think that explains the behavior I'm seeing.

    Sending the entire Robotiq script with each command does not sound very efficient; is there no efficient way to control the gripper over a socket while it's connected to the UR control box?

    It sounds like I should just connect the serial port of the gripper externally to the UR control box; is that what you'd recommend?
  • matthewd92matthewd92 Posts: 418 Handy
    Honestly, never tried controlling the gripper from off the robot.  When we do things like that we don't generally have a Robotiq on them.  

    How are the socket commands not being reliable?  We do quite a lot (rather did, replaced not too long ago with RPC) with socket commands and never had any issue with them.  We weren't controlling a gripper but communicating with an off-robot device over TCP/IP
  • jonlongjonlong Posts: 3 Apprentice
    Okay, I'm leaving URScript and switching to external control.

    What I meant about the socket commands is that simply calling "socket_set_var" over a URScript socket does not seem to reliably produce the expected response on the gripper (sometimes it does, sometimes nothing happens). The actual Robotiq implementation does a number of "sync" calls and has an ack-retry loop. I presume that that would work reliably, but again it's somewhat cumbersome to be sending that code as URScript for every gripper action...
  • cgilmercgilmer Posts: 9 Apprentice
    I have the exact same issue as you are having.  I would prefer to use the rq_* commands that I've seen shipped with the R85, but they are not available to me over a socket connection.  Currently I have to send individual "socket_set_var" commands to get the behavior I want and use a python time.sleep(2) command to block.

    For reference, I'm using and contributing to code here: https://github.com/SintefRaufossManufacturing/python-urx/blob/master/urx/robotiq_two_finger_gripper.py

    I'm currently reaching out to Robotiq to see if an engineer has a better idea of how to handle this situation.
  • matthewd92matthewd92 Posts: 418 Handy
    @cgilmer Since you are using an external library for robot control I am assuming you are also using an external computer, how about just hooking into the gripper directly from the PC?  You could just open the socket on the gripper and not have to go through the robot at all.  When we wrote the nodejs library similar to that one that was the plan we had for any external devices on the robot.  
  • cgilmercgilmer Posts: 9 Apprentice
    @matthewd92 - Interesting idea.  Can you link me to your node library?  Or is there a spec I can look at for socket communication to the gripper?  It's somewhat nice to go through the UR but not necessary.  If I could talk directly to the gripper I will probably have more control, which would be nice.
  • matthewd92matthewd92 Posts: 418 Handy
    @cgilmer we never implemented the Robotiq interface as we would up using an end effector we could operate via digital I/O and so just didn't need it for the project we were building the library for. It's actually still quite incomplete and we haven't opened it up to anyone outside our organization at this time but if there are some specifics you are interested in I can take a look at letting out small bits of the code. At some point when we have some more time to dedicate we'd like to get back on the project and open it up for some folks to help us with it. 

    As as far as communicating to the gripper here's some documentation on how to do that via Modbus RTU over either the USB to RS485 converter or directly via RS485. We're doing something similar on another project but we write all of our code in nodejs. The biggest difference with that project is we are strictly reading data so no writing to the registers but it looks rather straightforward just briefly reading over the docs. 

    http://support.robotiq.com/download/attachments/5963876/2-Finger-Instruction-Manual-060716.pdf?version=1&modificationDate=1467835896840&api=v2#page54
  • cgilmercgilmer Posts: 9 Apprentice
    This is actually super helpful.  It looks like the best way to manage the robotiq in this instance is to bypass the UR all together and just talk directly to it.  If I find time to do it, and if my company lets me, I'll try to open source the python driver when I get it done.
  • matthewd92matthewd92 Posts: 418 Handy
    edited February 9
    So I had a little spare time today so I sat down and started working on a nodejs library for controlling the 2F-85 gripper.  You can find the source code at https://github.com/mbush92/robotiq-node. Its very limited in scope currently as I just started knocking out some code this afternoon but you can activate the gripper and then open and close it.  If you're familiar with node you can run a simple script that I wrote called gripper.js in the /lib folder and it will control the gripper through an close and open cycle.  I will hopefully be doing some more work on this over the next few days.

    Hopefully it will give you guys some ideas on how to control the gripper using other languages as well.

    Also just as a note, I do not warranty the code to be free from errors or bugs so use at your own risk....had to throw that out there you know

    If anyone wants to work on this code as well let me know and I can add you as a contributor

  • cgilmercgilmer Posts: 9 Apprentice
    @matthewd92 - This library is great.  It looks like you talk directly on a serial connection to the gripper.  Have you figured out how to talk to the robotiq over an ethernet connection?
  • matthewd92matthewd92 Posts: 418 Handy
    @cgilmer Thanks, still a ways to go to make it really useable but it's a start.   Since it's a serial device I just talked to it directly. I plugged the USB cable directly into my mac.  Since it uses modbus RTU I'd think you would have to still somehow convert from TCP/IP to serial at some point to actually communicate to it

    Something that would be nice to have confirmed is if they all have the same address when you plug them in. I was able to find it pretty quick by looking in the /dev folder on my mac. @Etienne_Samson would you or one of the others have the answer to that question about the device address. 
  • PierreOlivier_ProulxPierreOlivier_Proulx Posts: 48 Handy
    edited February 13
    @matthewd92 The addresses of the usb/serial converter are assigned by the OS. So we cannot tell in advance how they will be named. On linux for example, they are named /dev/ttyUSBX or /dev/ttyACMX where X is an integer.

    @cgilmer For an external library to control Robotiq devices, have a look at the ros-industrial robotiq package. https://github.com/ros-industrial/robotiq. Use the gripper manual for the communication protocol description.
    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
  • @cglimer I re-read your post and regarding that quote "I would prefer to use the rq_* commands that I've seen shipped with the R85, but they are not available to me over a socket connection."  nothing prevents you from appending the gripper preamble to the urscript you are sending over tcp. This preamble declares the functions we use to control the gripper and you can find it in the .script file that is generated when you press the play button (those files are located next the .urp file in the programs directory).

    That preamble is quite long but you can probably prune it and keep only the relevant functions for your case.
    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
  • cgilmercgilmer Posts: 9 Apprentice
    @PierreOlivier_Proulx - I had tried appending the preamble to my script but it did not appear to work when I did it.  So for now I've left it out.  Instead I control the gripper state via UR script using socket_set_var and then put a timeout in my own code to simulate how long I expect it to take.  

    A better solution would be for me to talk directly over a socket connection to the gripper via the UR's built-in Modbus (as opposed to buying a separate modbus controller and connecting the gripper to it separately).  I haven't been able to do this yet or I haven't figured out how to set up the modbus on the polyscope correctly to allow it.

    My goals are really two-fold (and not exclusive):

    1. Cause a blocking action on the gripper action so that no other commands run while the gripper is in motion. (this is applicable probably only to my setup)
    2. Get the gripper state in real-time so I can figure out what's going on.  

    I haven't figured out how to do #1 (blocking action) so instead I have the timeout.  For #2, I think the variables I want get set globally and output on the primary monitor (the polyscope) but these same variables aren't sent out to the secondary monitor, which is what I'm using to monitor the robot and thus the gripper state.  I think this is more a problem with UR than with Robotiq.

    This brings me back to my initial wish - that I could control the robotiq directly over the UR modbus interface.  Any idea how to do this?


  • You can't control the gripper over UR modbus interface because UR client is ModbusTCP while the gripper is ModbusRTU (i.e. over a serial line). To do so you would have to buy a ModbusTCP controller to control the gripper.

    I still think that copying the whole preamble should work. URScript is very sensitive to indentation and it is not very verbose when problem occurs. Why not trying pasting the preamble but one function at a time to see the result incremantally.
    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
  • cgilmercgilmer Posts: 9 Apprentice
    @PierreOlivier_Proulx - You may have solved my problem.  What is the indentation rule that must be followed?  I bet my indentation was wrong and so it errored out.
  • PierreOlivier_ProulxPierreOlivier_Proulx Posts: 48 Handy
    edited February 14
    The particularity is that function definitions cannot be on the same indentation level as the program definition. However, regular instruction can. This might look obvious but we had situations where we were having a functional script with built-in instructions on level 0 and then, after adding a function nothing worked. You also have to be careful with the : at the end of control instructions (if, while, function) and the end that close those control instructions block. As a general rule, when I have to write a script by hand, I usually do it very incrementally, testing every small modification in order to catch problems early.
    <div>def prog():&nbsp;
     def func():&nbsp;
     textmsg("abc")&nbsp;
     end&nbsp;
    func()&nbsp;
    end
    </div>
    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
  • cgilmercgilmer Posts: 9 Apprentice
    @PierreOlivier_Proulx - I'm going to try this out.  It's super helpful.  Thanks for sharing this with me.  I'll let you know if it works sometime in the next couple days when I get back to it.
  • @cgilmer I took a look at the repo you linked https://github.com/SintefRaufossManufacturing/python-urx/blob/master/urx/robotiq_two_finger_gripper.py. I think that you could directly add the gripper preamble in that file and use rq_* functions directly instead of socket_set_var.

    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
  • cgilmercgilmer Posts: 9 Apprentice
    @PierreOlivier_Proulx - I think you're right.  one other question: do you know if the URScript is sensitive to tabs or spaces?  I assume it requires tabs.  But if you know it would help tremendously.
  • PierreOlivier_ProulxPierreOlivier_Proulx Posts: 48 Handy
    edited February 14
    @cgilmer I always use spaces.
    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
  • cgilmercgilmer Posts: 9 Apprentice
  • matthewd92matthewd92 Posts: 418 Handy
    I've found that it doesn't matter either way, tabs though seem to be pretty indented. 
  • @cgilmer take a look at this fork, I appended the preamble.
    Pierre-Olivier Proulx
    Software Designer
    poproulx@robotiq.com
Sign In or Register to comment.
Left ArrowBack to discussions page