@afritz your gripper should be able to detect anything over 1.2mm thickness, even if you did custom fingertips, could you show us your setup with some photos ? Maybe send a sample of your program ?
Etienne_Samson
@afritz those fingertips exceed our maximum dimensions specified in the manual. The object detection will be less reliable due to the deformation of those fingertips, in order to have a reliable detection they would need to be perfectly rigid. Gripper force will be affected too, and Gripper maintenance requirement will be increased.
You could indeed use the FT sensor to detect the weight of the object, it would be fairly easy. You read the Mx or My signal and use the length of that setup as a lever to estimate what mass is present or not. This is commonly used for quality inspection applications, it works.

matthewd92
Hello everyone,
i'm Ariane from Germany and i'm very new to robotics(2weeks). I m working with UR10 in combination with 2 finger Gripper und FT 150 Sensor.
At our company we want to grab Carrier from an tower and bring it to a spindle for a show case. So we extended the gripper arm with two metal plates (screwed on the gripper up and down).
Now the gripper does not detect any object, that are only fetched by the plates... or he might squeezed the carrier before he marked it as detected
Is there any possibily to augment the sensivity of the gripper or the FT 150? Or should i write any program code to talk directly with the sensor or it is not possible...
Thanks a lot for your help
Best regards