Discussion

Left ArrowBack to discussions page
JonnoJonno Posts: 2 Recruit
edited January 4 in Robotiq Products
Hello,
I'm having an issue with the reflection in the part I am trying to pick up is being caused by the flash on the camera. Is there anyway to turn the flash off? 

I am running software 1.0.2. 
I tried 1.1.1 but it was causing lots more issues. 

Thanks
Jonno

Comments

  • Annick_MottardAnnick_Mottard Posts: 109 Handy
    @Jonno just opened up a support ticket for this situation. What further issues are you getting with the 1.1.1 version? Concerning the reflection on your part, you can refer to this DoF post, as well as this one.
    Annick Mottard
    Product Expert
    Robotiq
    a.mottard@robotiq.com 
  • JonnoJonno Posts: 2 Recruit

    We are having issues with the calibration. When we calibrate it shows an error saying that there isn't enough reachable positions. Also if we use the same calibration from the previous software, when teaching the part it comes up with the same issue. These positions work with software 1.0.2.

    Could you send me the .rar file for 1.0.2 please?


  • Etienne_SamsonEtienne_Samson Posts: 319 Handy
    @Jonno to follow-up on this, I explained your colleague Matt that the calibration and the snapshot position does not have to be the same. That's the trick, and the software doesn't explicitly tells you.

    Keep your Snapshot position there, it's fine.

    On the Calibration step, move the board away (but on the same plane) on some place were the robot will have enough reach to scan the board. Move the robot, stay away from singularities and start the calibration.

    The only thing you need to keep is the plane, the calibration board must be on the same plane with same height then the Snapshot position will be looking at, but beside that it can be anywhere else.
    Etienne Samson
    Technical Support Manager - Responsable soutien technique
    +01 418-380-2788 ext. 207
    esamson@robotiq.com
Sign In or Register to comment.
Left ArrowBack to discussions page