Discussion

Left ArrowBack to discussions page
ericeric Posts: 18Founding Pro, Partner Handy
edited December 2016 in Applications
Is anyone doing any explosion proof painting applications with the Universal Robot?

Comments

  • SebastienSebastien Posts: 194 Handy
    @eric
    We looked at this a bit a tried to see if anyone could provide an explosion proof suit for the UR robot. The main feature of explosion proof robots like Fanuc is that they have a constant air pressure flowing in the robot arm to keep fumes outside the robot mechanical unit. So it feasible to have a suite that would keep a certain air pressure level inside. However, it seems like no one did the explosion proof certification for such a suit.

    Hope that helps!
Sign In or Register to comment.
Left ArrowBack to discussions page