DoF - a Robotiq Community
Warning sign
The Dof Community was shut down in June 2023. This is a read-only archive.
If you have questions about Robotiq products please reach our support team.
Achaniotis

@Achaniotis would that be constant temperature or would it be the part/peak temperature ? Our Gripper cannot work at a constant temperature of 480°C, if the part is at 480 we can probably work something with the fingers to have it running fine. Otherwise there are other solutions on the market but an electric gripper like ours could not handle ambiant conditions like this.

480°C will be the part temperature after it comes out of a pre-heating furnace. I am assuming that the part will not spend more than a few seconds in contact with the gripper. The temperature of the working environment will be at normal industrial levels.