DoF - a Robotiq Community
Warning sign
The Dof Community was shut down in June 2023. This is a read-only archive.
If you have questions about Robotiq products please reach our support team.
matthewd92

I have done vision based inspection in the past using Cognex. The way it works is you will build a vision program that has the features that you want to inspect. Often you will use a feature on the part to orient the inspection frame of reference to the actual part orientation. This allows for the part to move slightly and still the vision system to locate the part. Then it's just a matter of adding various tools to the program for measuring the features you are interested in. The really great thing about vision inspection is it's extremely fast. We used to measure about 10 different features on the parts we made at a rate of more than 90 per minute and we could decide whether a part was good or bad and reject or accept accordingly. We had trap doors in the part chute that would open on rejected parts. Under the trap door would be a light curtain that we used to verify that the rejected part exited the chute. Then the door would close and the machine would continue. All of this was happening as we were making parts at around 94 per minute. 

We we also used vision to inspect ink jet printing on stainless steel strip moving at roughly 1000 feet per minute. The camera would read the message that was printed about every 8" and then either accept the lettering or spray a reject mark onto the band that the machine would use to reject the bad section of band. 

Cognex, Microscan, Sensopart, Keyence and others all make vision inspection systems. Prices can vary from $2000 to close to $10000 or possibly more depending on what you need to do exactly what you are trying to accomplish. Lighting is extremely important and can be a little like black magic. 

I'm sure there are other pros that can chime in on this as well.