Discussion

Left ArrowBack to discussions page
matthewd92matthewd92 Posts: 477Founding Pro, Tactile Sensor Beta Testers Handy
edited August 2016 in Integration
We have an application where I need to have a tool changer on the UR5 so that we can switch between tools during operation.  Has anyone used either the ATI or Schunk system with the UR robots?  If so, what was your experience with it?

Best Answer

Comments

  • Samuel_BouchardSamuel_Bouchard Posts: 136 Handy
    @Catherine_Bernier @Alexandre_Pare @Nicolas_Hardy you have some people who you know could jump in this discussion?



    CEO & Co-Founder @ Robotiq

    samuel@robotiq.com
  • Alexandre_PareAlexandre_Pare Posts: 56 Crew
    @matthewd92
    I have not seen much clients using tool changers on UR robots. Most clients using tool changers were on industrial robots such as Fanuc, Kuka and so on. I don't see any issues with this on the UR though. I think that the repeatability of the UR is good enough to perform tool change. I think that force mode of the UR could also be used to ensure proper tool changes.

    Alexandre Pare, Eng.
    Application Engineer
    Robotiq
    alexandre.pare@robotiq.com
  • Johnson_LiuJohnson_Liu Posts: 10Founding Pro Handy

    @matthewd92, In Taiwan, we sold Gripper 85 & RSP(Robot Sysytem Products - Sweden company spin-off from ABB) tool changers (TC20/TA20) with UR robot to Toyota Motor early of this year, and we also sold ATI tool changers to industrial robot customer- e.g ABB robot end users, most of robots brand could suitable with ATI, RSP or Schunk, the key point is chosing the right tool changer payload and fitted with robots and applications, also the air channels, electricl signals or power need to considering when connect to outside tooling (e.g air spindles, or electrical spindles when deburring, cutting, or routing). We have some successful applications in selling the ATI/RSP tool changers with industrial robots, especially for ABB and Funac robots in past years, of course the UR robots could using the tool changers on different applications.

    Johnson Liu

    Robotics & 3A Inc. www.twin-robotics.com  

  • matthewd92matthewd92 Posts: 477Founding Pro, Tactile Sensor Beta Testers Handy
    @Johnson_Liu thanks for the information!
  • matthewd92matthewd92 Posts: 477Founding Pro, Tactile Sensor Beta Testers Handy
    So I thought this was interesting. Last week at IMTS I learned from one of the Schunk guys that they actually source their small tool changers from ATI. His comment was the main reason to buy from Schunk would be to have a one stop shop for the changer and gripper. Now I don't know if this means they are the exact same unit or just ATI produces them. But either way thought I'd share. 
Sign In or Register to comment.
Left ArrowBack to discussions page