DoF - a Robotiq Community
Warning sign
The Dof Community was shut down in June 2023. This is a read-only archive.
If you have questions about Robotiq products please reach our support team.
Catherine_Bernier

When using DeviceNet protocol, it is very important to have resistors located on both end of the communication cable. Those resistors are also called end-of-line devices.

According to
odva.org:

The terminating resistor reduces reflections of the communication signals on the network.

Attention:  If you do not use terminating resistors as described, the DeviceNet (TM) cable system will not operate properly.
It is recommended to use 120 ohms resistors. In an integrated robotic system, the further device to add the resistor to is often the end-of-arm tool.

Make sure to consider this in your next DeviceNet integration.